Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static LawBuilder.RetainLawCurveOption |
LawBuilder.RetainLawCurveOption.KEEP_ORIGINAL
Keeps the original profile as it is during edit pre NX3 parms
|
static LawBuilder.RetainLawCurveOption |
LawBuilder.RetainLawCurveOption.REPLACE
Deletes the old profile, so that user has to select new one during edit pre NX3 parms
|
Modifier and Type | Method and Description |
---|---|
LawBuilder.RetainLawCurveOption |
LawBuilder.lawCurveOption()
Returns the option to retain law curve.
|
static LawBuilder.RetainLawCurveOption |
LawBuilder.RetainLawCurveOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static LawBuilder.RetainLawCurveOption |
LawBuilder.RetainLawCurveOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static LawBuilder.RetainLawCurveOption[] |
LawBuilder.RetainLawCurveOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
LawBuilder.setLawCurveOption(LawBuilder.RetainLawCurveOption lawCurveOption)
License requirements: solid_modeling ("SOLIDS MODELING") OR drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.