Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
InstanceEditedExpressionItem |
InstanceEditedExpressionsList.editInstanceExpression()
This is the default creator for
InstanceEditedExpressionItem . |
InstanceEditedExpressionItem |
InstanceEditedExpressionsList.editInstanceExpression(Expression masterExpression,
Expression instanceExpression)
This is the creator for
InstanceEditedExpressionItem which should be used. |
InstanceEditedExpressionItem |
InstanceEditedExpressionItemList.findItem(int index)
Returns the object at the input index.
|
InstanceEditedExpressionItem[] |
InstanceEditedExpressionItemList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
InstanceEditedExpressionItemList.append(InstanceEditedExpressionItem object)
Appends an object to the list
License requirements: None. |
void |
InstanceEditedExpressionItemList.append(InstanceEditedExpressionItem[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
InstanceEditedExpressionItemList.erase(InstanceEditedExpressionItem obj)
Erases the object from the list, but does not delete the object.
|
void |
InstanceEditedExpressionItemList.erase(InstanceEditedExpressionItem obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
InstanceEditedExpressionItemList.findIndex(InstanceEditedExpressionItem obj)
Finds the index where the input object appears.
|
void |
InstanceEditedExpressionItemList.insert(int location,
InstanceEditedExpressionItem object)
Inserts an object at the specified location
License requirements: None. |
void |
InstanceEditedExpressionItemList.setContents(InstanceEditedExpressionItem[] objects)
Sets the contents of the entire list.
|
void |
InstanceEditedExpressionItemList.swap(InstanceEditedExpressionItem object1,
InstanceEditedExpressionItem object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.