Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static HelixPattern.SizeOptions |
HelixPattern.SizeOptions.ANGLE_HELIX_PITCH_AND_SPAN
use Angle, Helix Pitch, Span to define a Helix
|
static HelixPattern.SizeOptions |
HelixPattern.SizeOptions.ANGLE_HELIX_PITCH_AND_TURNS
use Angle, Helix Pitch, Turns to define a Helix
|
static HelixPattern.SizeOptions |
HelixPattern.SizeOptions.COUNT_ANGLE_DISTANCE
use Count, Angle, Distance to define a Helix
|
static HelixPattern.SizeOptions |
HelixPattern.SizeOptions.COUNT_HELIX_PITCH_AND_SPAN
use Count, Helix Pitch, Span to define a Helix
|
static HelixPattern.SizeOptions |
HelixPattern.SizeOptions.COUNT_HELIX_PITCH_AND_TURNS
use Count, Helix Pitch, Turns to define a Helix
|
Modifier and Type | Method and Description |
---|---|
HelixPattern.SizeOptions |
HelixPattern.sizeOption()
Returns the Helix size option
License requirements: None. |
static HelixPattern.SizeOptions |
HelixPattern.SizeOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HelixPattern.SizeOptions |
HelixPattern.SizeOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HelixPattern.SizeOptions[] |
HelixPattern.SizeOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HelixPattern.setSizeOption(HelixPattern.SizeOptions option)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.