Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static GeneralPattern.FromLocationOptions |
GeneralPattern.FromLocationOptions.CSYS
csys
|
static GeneralPattern.FromLocationOptions |
GeneralPattern.FromLocationOptions.POINT
point
|
Modifier and Type | Method and Description |
---|---|
GeneralPattern.FromLocationOptions |
GeneralPattern.fromLocationType()
Returns the from location type
License requirements: None. |
static GeneralPattern.FromLocationOptions |
GeneralPattern.FromLocationOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GeneralPattern.FromLocationOptions |
GeneralPattern.FromLocationOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GeneralPattern.FromLocationOptions[] |
GeneralPattern.FromLocationOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GeneralPattern.setFromLocationType(GeneralPattern.FromLocationOptions fromLocationType)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.