Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
FtmFixedCurvesBuilder |
OmnicadManager.createFtmFixedCurvesBuilder()
Creates Free Transformer fixed curves builder.
|
FtmFixedCurvesBuilder |
FtmFixedCurvesBuilderList.findItem(int index)
Returns the object at the input index.
|
FtmFixedCurvesBuilder[] |
FtmFixedCurvesBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
FtmFixedCurvesBuilderList.append(FtmFixedCurvesBuilder object)
Appends an object to the list
License requirements: None. |
void |
FtmFixedCurvesBuilderList.append(FtmFixedCurvesBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
FtmFixedCurvesBuilderList.erase(FtmFixedCurvesBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
FtmFixedCurvesBuilderList.erase(FtmFixedCurvesBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
FtmFixedCurvesBuilderList.findIndex(FtmFixedCurvesBuilder obj)
Finds the index where the input object appears.
|
void |
FtmFixedCurvesBuilderList.insert(int location,
FtmFixedCurvesBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
FtmFixedCurvesBuilderList.setContents(FtmFixedCurvesBuilder[] objects)
Sets the contents of the entire list.
|
void |
FtmFixedCurvesBuilderList.swap(FtmFixedCurvesBuilder object1,
FtmFixedCurvesBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.