Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static FrameOnPathBuilder.AnchorLocationType |
FrameOnPathBuilder.AnchorLocationType.CENTER
Center position
|
static FrameOnPathBuilder.AnchorLocationType |
FrameOnPathBuilder.AnchorLocationType.LEFT
Left position
|
static FrameOnPathBuilder.AnchorLocationType |
FrameOnPathBuilder.AnchorLocationType.RIGHT
Right position
|
Modifier and Type | Method and Description |
---|---|
FrameOnPathBuilder.AnchorLocationType |
FrameOnPathBuilder.anchorLocation()
Returns the anchor location
License requirements: None. |
static FrameOnPathBuilder.AnchorLocationType |
FrameOnPathBuilder.AnchorLocationType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FrameOnPathBuilder.AnchorLocationType |
FrameOnPathBuilder.AnchorLocationType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FrameOnPathBuilder.AnchorLocationType[] |
FrameOnPathBuilder.AnchorLocationType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FrameOnPathBuilder.setAnchorLocation(FrameOnPathBuilder.AnchorLocationType anchorLocation)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.