Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static FlowDirection.Type |
FlowDirection.Type.ADJACENT_EDGES
Adjacent Edges
|
static FlowDirection.Type |
FlowDirection.Type.ISO_CURVE_U
Iso Curve U
|
static FlowDirection.Type |
FlowDirection.Type.ISO_CURVE_V
Iso Curve V
|
static FlowDirection.Type |
FlowDirection.Type.ISOPARAMETRIC
Iso Parametric
|
static FlowDirection.Type |
FlowDirection.Type.NOT_SPECIFIED
Not Specified
|
static FlowDirection.Type |
FlowDirection.Type.PERPENDICULAR
Perpendicular
|
Modifier and Type | Method and Description |
---|---|
FlowDirection.Type |
FlowDirection.flowDirectionType()
Returns the flow direction type.
|
static FlowDirection.Type |
FlowDirection.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FlowDirection.Type |
FlowDirection.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FlowDirection.Type[] |
FlowDirection.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FlowDirection.setFlowDirectionType(FlowDirection.Type flowDirectionType)
License requirements: nx_freeform_1 ("basic freeform modeling") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.