Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static EndHoleData.ThreadLengthOptions |
EndHoleData.ThreadLengthOptions.CUSTOM
Length is custom
|
static EndHoleData.ThreadLengthOptions |
EndHoleData.ThreadLengthOptions.DIAMETERX1
1 * (tap drill diameter)
|
static EndHoleData.ThreadLengthOptions |
EndHoleData.ThreadLengthOptions.DIAMETERX15
1.5 * (tap drill diameter)
|
static EndHoleData.ThreadLengthOptions |
EndHoleData.ThreadLengthOptions.DIAMETERX20
2 * (tap drill diameter)
|
static EndHoleData.ThreadLengthOptions |
EndHoleData.ThreadLengthOptions.DIAMETERX25
2.5 * (tap drill diameter)
|
static EndHoleData.ThreadLengthOptions |
EndHoleData.ThreadLengthOptions.DIAMETERX30
3 * (tap drill diameter)
|
static EndHoleData.ThreadLengthOptions |
EndHoleData.ThreadLengthOptions.FULL
Length is full hole depth
|
static EndHoleData.ThreadLengthOptions |
EndHoleData.ThreadLengthOptions.STANDARD
Length is standard
|
Modifier and Type | Method and Description |
---|---|
EndHoleData.ThreadLengthOptions |
EndHoleData.threadLengthOption()
Returns the thread length option
License requirements: None. |
static EndHoleData.ThreadLengthOptions |
EndHoleData.ThreadLengthOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EndHoleData.ThreadLengthOptions |
EndHoleData.ThreadLengthOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EndHoleData.ThreadLengthOptions[] |
EndHoleData.ThreadLengthOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EndHoleData.setThreadLengthOption(EndHoleData.ThreadLengthOptions threadLengthOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.