Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static EndHoleData.FormOptions |
EndHoleData.FormOptions.SCREW_CLEARANCE
Screw clearance
|
static EndHoleData.FormOptions |
EndHoleData.FormOptions.THREADED
Threaded hole
|
static EndHoleData.FormOptions |
EndHoleData.FormOptions.THROUGH
Through hole - This option should not be used in NX6 and later versions.
|
Modifier and Type | Method and Description |
---|---|
EndHoleData.FormOptions |
EndHoleData.formOption()
Returns the form option
License requirements: None. |
static EndHoleData.FormOptions |
EndHoleData.FormOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static EndHoleData.FormOptions |
EndHoleData.FormOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static EndHoleData.FormOptions[] |
EndHoleData.FormOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
EndHoleData.setFormOption(EndHoleData.FormOptions formOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.