Package | Description |
---|---|
nxopen |
Provides classes and interfaces for the NX Open Common API.
|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Method and Description |
---|---|
BoundaryDefinitionBuilder |
Part.createEmptyBoundaryDefinitionBuilder()
Creates boundary definition builder object
License requirements: studio_free_form ("STUDIO FREE FORM") . |
Modifier and Type | Method and Description |
---|---|
BoundaryDefinitionBuilder |
BoundaryDefinitionBuilderList.findItem(int index)
Returns the object at the input index.
|
BoundaryDefinitionBuilder[] |
BoundaryDefinitionBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
BoundaryDefinitionBuilderList.append(BoundaryDefinitionBuilder object)
Appends an object to the list
License requirements: None. |
void |
BoundaryDefinitionBuilderList.append(BoundaryDefinitionBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
BoundaryDefinitionBuilderList.erase(BoundaryDefinitionBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
BoundaryDefinitionBuilderList.erase(BoundaryDefinitionBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
BoundaryDefinitionBuilderList.findIndex(BoundaryDefinitionBuilder obj)
Finds the index where the input object appears.
|
void |
BoundaryDefinitionBuilderList.insert(int location,
BoundaryDefinitionBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
BoundaryDefinitionBuilderList.setContents(BoundaryDefinitionBuilder[] objects)
Sets the contents of the entire list.
|
void |
BoundaryDefinitionBuilderList.swap(BoundaryDefinitionBuilder object1,
BoundaryDefinitionBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.