Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static BooleanRegionSelect.SelectOption |
BooleanRegionSelect.SelectOption.KEEP_AND_REMOVE
Keep and remove regions
|
static BooleanRegionSelect.SelectOption |
BooleanRegionSelect.SelectOption.KEEP_OR_REMOVE
Keep or remove regions
|
static BooleanRegionSelect.SelectOption |
BooleanRegionSelect.SelectOption.NONE
No regions to pick
|
Modifier and Type | Method and Description |
---|---|
BooleanRegionSelect.SelectOption |
BooleanRegionSelect.selectMethod()
Returns the boolean region selection method method
License requirements: None. |
static BooleanRegionSelect.SelectOption |
BooleanRegionSelect.SelectOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BooleanRegionSelect.SelectOption |
BooleanRegionSelect.SelectOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BooleanRegionSelect.SelectOption[] |
BooleanRegionSelect.SelectOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BooleanRegionSelect.setSelectMethod(BooleanRegionSelect.SelectOption selectOption)
License requirements: solid_modeling ("SOLIDS MODELING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.