Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static BooleanOperation.BooleanType |
BooleanOperation.BooleanType.CREATE
Create
|
static BooleanOperation.BooleanType |
BooleanOperation.BooleanType.INTERSECT
Intersect
|
static BooleanOperation.BooleanType |
BooleanOperation.BooleanType.SEW
Sew
|
static BooleanOperation.BooleanType |
BooleanOperation.BooleanType.SUBTRACT
Subtract
|
BooleanOperation.BooleanType |
BooleanOperation.BooleanOperationAndBodyData.type
boolean type
|
static BooleanOperation.BooleanType |
BooleanOperation.BooleanType.UNITE
Unite
|
Modifier and Type | Method and Description |
---|---|
BooleanOperation.BooleanType |
BooleanOperation.type()
Returns the boolean operation type
License requirements: None. |
static BooleanOperation.BooleanType |
BooleanOperation.BooleanType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BooleanOperation.BooleanType |
BooleanOperation.BooleanType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BooleanOperation.BooleanType[] |
BooleanOperation.BooleanType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BooleanOperation.setBooleanOperationAndBody(BooleanOperation.BooleanType type,
Body targetBody)
Deprecated.
Deprecated in NX4.0.0. Use
BooleanOperation.setType(nxopen.geometricutilities.BooleanOperation.BooleanType) and BooleanOperation.setTargetBodies(nxopen.Body[]) instead.
|
void |
BooleanOperation.setType(BooleanOperation.BooleanType type)
License requirements: solid_modeling ("SOLIDS MODELING") OR cam_base ("CAM BASE") OR insp_programming ("INSPECTION PROGRAMMING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.