Package | Description |
---|---|
nxopen.geometricutilities |
Provides classes and interfaces for Geometric Utilities.
|
Modifier and Type | Field and Description |
---|---|
static AngularPatternSpacing.UsePitchOptions |
AngularPatternSpacing.UsePitchOptions.ANGLE
angle is pitch value
|
static AngularPatternSpacing.UsePitchOptions |
AngularPatternSpacing.UsePitchOptions.DISTANCE
distance is pitch value.
|
Modifier and Type | Method and Description |
---|---|
AngularPatternSpacing.UsePitchOptions |
AngularPatternSpacing.usePitchOption()
Returns the switch to use Pitch Distance or Pitch Angle.
|
static AngularPatternSpacing.UsePitchOptions |
AngularPatternSpacing.UsePitchOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static AngularPatternSpacing.UsePitchOptions |
AngularPatternSpacing.UsePitchOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static AngularPatternSpacing.UsePitchOptions[] |
AngularPatternSpacing.UsePitchOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
AngularPatternSpacing.setUsePitchOption(AngularPatternSpacing.UsePitchOptions usePitchOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.