public static class Rebuild.DegreeTypes extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_CUBIC
The rebuild degree is cubic.
|
static int |
_QUINTIC
The rebuild degree is quintic
|
static Rebuild.DegreeTypes |
CUBIC
The rebuild degree is cubic.
|
static Rebuild.DegreeTypes |
QUINTIC
The rebuild degree is quintic
|
Modifier and Type | Method and Description |
---|---|
static Rebuild.DegreeTypes |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static Rebuild.DegreeTypes |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static Rebuild.DegreeTypes[] |
values()
Returns an array that contains the values for this enum.
|
public static final Rebuild.DegreeTypes CUBIC
public static final Rebuild.DegreeTypes QUINTIC
public static final int _CUBIC
public static final int _QUINTIC
public static Rebuild.DegreeTypes valueOf(int value)
public static Rebuild.DegreeTypes valueOf(String name)
public static Rebuild.DegreeTypes[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.