public static class PatternIncrementItem.OperationEnum extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ADD
add the increment to the master value.
|
static int |
_MULTIPLY
multiply the increment to the master value.
|
static PatternIncrementItem.OperationEnum |
ADD
add the increment to the master value.
|
static PatternIncrementItem.OperationEnum |
MULTIPLY
multiply the increment to the master value.
|
Modifier and Type | Method and Description |
---|---|
static PatternIncrementItem.OperationEnum |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PatternIncrementItem.OperationEnum |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PatternIncrementItem.OperationEnum[] |
values()
Returns an array that contains the values for this enum.
|
public static final PatternIncrementItem.OperationEnum ADD
public static final PatternIncrementItem.OperationEnum MULTIPLY
public static final int _ADD
public static final int _MULTIPLY
public static PatternIncrementItem.OperationEnum valueOf(int value)
public static PatternIncrementItem.OperationEnum valueOf(String name)
public static PatternIncrementItem.OperationEnum[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.