public static class BridgeCurveConnectivity.FaceDirectionOptions extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ISO_U
Along U iso-parameter
|
static int |
_ISO_V
Along V iso-parameter
|
static int |
_SECTIONAL
Sectional direction
|
static BridgeCurveConnectivity.FaceDirectionOptions |
ISO_U
Along U iso-parameter
|
static BridgeCurveConnectivity.FaceDirectionOptions |
ISO_V
Along V iso-parameter
|
static BridgeCurveConnectivity.FaceDirectionOptions |
SECTIONAL
Sectional direction
|
Modifier and Type | Method and Description |
---|---|
static BridgeCurveConnectivity.FaceDirectionOptions |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BridgeCurveConnectivity.FaceDirectionOptions |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BridgeCurveConnectivity.FaceDirectionOptions[] |
values()
Returns an array that contains the values for this enum.
|
public static final BridgeCurveConnectivity.FaceDirectionOptions SECTIONAL
public static final BridgeCurveConnectivity.FaceDirectionOptions ISO_U
public static final BridgeCurveConnectivity.FaceDirectionOptions ISO_V
public static final int _SECTIONAL
public static final int _ISO_U
public static final int _ISO_V
public static BridgeCurveConnectivity.FaceDirectionOptions valueOf(int value)
public static BridgeCurveConnectivity.FaceDirectionOptions valueOf(String name)
public static BridgeCurveConnectivity.FaceDirectionOptions[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.