Package | Description |
---|---|
nxopen.geometricanalysis.sectionanalysis |
Provides classes and interfaces for Section Analysis.
|
Modifier and Type | Field and Description |
---|---|
static SectionAnalysisExBuilder.AlignmentType |
SectionAnalysisExBuilder.AlignmentType.CURVE_ALIGNED
The cutting planes are perpendicular to specified curves
|
static SectionAnalysisExBuilder.AlignmentType |
SectionAnalysisExBuilder.AlignmentType.ISOPARAMETRIC
The sections are along isoparametric lines
|
static SectionAnalysisExBuilder.AlignmentType |
SectionAnalysisExBuilder.AlignmentType.PARALLEL_PLANES
The cutting planes are parallel to a specified plane
|
static SectionAnalysisExBuilder.AlignmentType |
SectionAnalysisExBuilder.AlignmentType.RADIAL
The cutting planes are distributed along a circle
|
static SectionAnalysisExBuilder.AlignmentType |
SectionAnalysisExBuilder.AlignmentType.XYZPLANE
The cutting planes are perpendicular to X, Y or Z plane
|
Modifier and Type | Method and Description |
---|---|
SectionAnalysisExBuilder.AlignmentType |
SectionAnalysisExBuilder.alignment()
Returns the alignment type
License requirements: None. |
static SectionAnalysisExBuilder.AlignmentType |
SectionAnalysisExBuilder.AlignmentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SectionAnalysisExBuilder.AlignmentType |
SectionAnalysisExBuilder.AlignmentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SectionAnalysisExBuilder.AlignmentType[] |
SectionAnalysisExBuilder.AlignmentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SectionAnalysisExBuilder.setAlignment(SectionAnalysisExBuilder.AlignmentType alignment)
License requirements: studio_analyze ("STUDIO ANALYZE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.