Package | Description |
---|---|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
Modifier and Type | Field and Description |
---|---|
static ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.NumberOfLinesOptions.EIGHT
8 reflection line.
|
static ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.NumberOfLinesOptions.FOUR
4 reflection line.
|
static ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.NumberOfLinesOptions.ONE
1 reflection line.
|
static ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.NumberOfLinesOptions.ONE_TWO_EIGHT
128 reflection line.
|
static ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.NumberOfLinesOptions.SIXTEEN
16 reflection line.
|
static ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.NumberOfLinesOptions.SIXTY_FOUR
64 reflection line.
|
static ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.NumberOfLinesOptions.THIRTY_TWO
32 reflection line.
|
static ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.NumberOfLinesOptions.TWO
2 reflection line.
|
static ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.NumberOfLinesOptions.TWO_FIVE_SIX
256 reflection line.
|
Modifier and Type | Method and Description |
---|---|
ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.lineNumber()
Returns the reflection line number.
|
static ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.NumberOfLinesOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ReflectionAnalysisBuilder.NumberOfLinesOptions |
ReflectionAnalysisBuilder.NumberOfLinesOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ReflectionAnalysisBuilder.NumberOfLinesOptions[] |
ReflectionAnalysisBuilder.NumberOfLinesOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ReflectionAnalysisBuilder.setLineNumber(ReflectionAnalysisBuilder.NumberOfLinesOptions lineNumber)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.