Package | Description |
---|---|
nxopen.geometricanalysis |
Provides classes and interfaces for Geometric Analysis.
|
Modifier and Type | Field and Description |
---|---|
static HighlightLinesAnalysisBuilder.LightPlacements |
HighlightLinesAnalysisBuilder.LightPlacements.BETWEEN_POINTS
Between Points: Two highlight lines are guaranteed to
pass through two given surface points.
|
static HighlightLinesAnalysisBuilder.LightPlacements |
HighlightLinesAnalysisBuilder.LightPlacements.THROUGH_POINTS
Through Points: A highlight line is guaranteed to pass through a surface point.
|
static HighlightLinesAnalysisBuilder.LightPlacements |
HighlightLinesAnalysisBuilder.LightPlacements.UNIFORM
Uniform: Lights are placed uniformly on light plane
|
Modifier and Type | Method and Description |
---|---|
HighlightLinesAnalysisBuilder.LightPlacements |
HighlightLinesAnalysisBuilder.lightPlacement()
Returns the light placement
License requirements: None. |
static HighlightLinesAnalysisBuilder.LightPlacements |
HighlightLinesAnalysisBuilder.LightPlacements.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HighlightLinesAnalysisBuilder.LightPlacements |
HighlightLinesAnalysisBuilder.LightPlacements.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HighlightLinesAnalysisBuilder.LightPlacements[] |
HighlightLinesAnalysisBuilder.LightPlacements.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HighlightLinesAnalysisBuilder.setLightPlacement(HighlightLinesAnalysisBuilder.LightPlacements placement)
License requirements: studio_analyze ("STUDIO ANALYZE") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.