Package | Description |
---|---|
nxopen.gateway |
Provides classes and interfaces for Gateway.
|
Modifier and Type | Field and Description |
---|---|
static ImageCaptureBuilder.CaptureMethodType |
ImageCaptureBuilder.CaptureMethodType.AUTOMATIC
the automatic preview mode
|
static ImageCaptureBuilder.CaptureMethodType |
ImageCaptureBuilder.CaptureMethodType.FILE
the input from file
|
static ImageCaptureBuilder.CaptureMethodType |
ImageCaptureBuilder.CaptureMethodType.GRAPHICS_AREA
the graphics area
|
static ImageCaptureBuilder.CaptureMethodType |
ImageCaptureBuilder.CaptureMethodType.REGION
the region area
|
Modifier and Type | Method and Description |
---|---|
ImageCaptureBuilder.CaptureMethodType |
ImageCaptureBuilder.captureMethod()
Returns the capture method
License requirements: None. |
static ImageCaptureBuilder.CaptureMethodType |
ImageCaptureBuilder.CaptureMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ImageCaptureBuilder.CaptureMethodType |
ImageCaptureBuilder.CaptureMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ImageCaptureBuilder.CaptureMethodType[] |
ImageCaptureBuilder.CaptureMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ImageCaptureBuilder.setCaptureMethod(ImageCaptureBuilder.CaptureMethodType captureMethod)
License requirements: drafting ("DRAFTING") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.