Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.fields |
Provides classes and interfaces for Fields.
|
Modifier and Type | Interface and Description |
---|---|
interface |
FemSignalProcessingSignalAttributes
Implementation of the
IApplicationData . |
Modifier and Type | Method and Description |
---|---|
IApplicationData |
Field.getApplicationData(String applicationName)
Retrieves the application data associated with the field for the specified application.
|
Modifier and Type | Method and Description |
---|---|
void |
Field.addApplicationData(IApplicationData applicationData)
Adds the specified application data object to the field
NOTE: Only one application data object per IApplication can be added
and the data must be owned by an IApplication with the same Part::Field::Main
as the field.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.