Package | Description |
---|---|
nxopen.cae |
Provides classes and interfaces relating to Advanced Simulation and Design Simulation.
|
nxopen.fields |
Provides classes and interfaces for Fields.
|
Modifier and Type | Method and Description |
---|---|
FieldTable |
ResultManager.createTableFieldForModel(String fieldName,
int indepDomainType,
int depDomainType,
int nodevalshare,
int pvid,
boolean isdeform,
int[] elem,
boolean includeOrExculde)
Creates a table for the model.
|
FieldTable |
PostGraphBuilder.getFieldTable()
Gets the field which is created when user sets the
PostGraphBuilder.createFieldOption() and PostGraphBuilder.setCreateFieldOption(boolean)
to true for across iterations type of graphs
License requirements: nx_masterfem ("Finite Element Modeling") OR nx_design_sim ("NX Design Simulation") OR sc_results_viewer (" Simcenter Results Viewer") Created in NX9.0.0 |
Modifier and Type | Interface and Description |
---|---|
interface |
FieldProfileTable
Represents the Field Profile class.
|
Modifier and Type | Method and Description |
---|---|
FieldTable |
FieldManager.createFieldTable(String fieldName,
FieldVariable[] indepVarArray,
FieldVariable[] depVarArray,
double[] datapoints)
Creates a
FieldTable object with dependent and independent variables
FieldVariable . |
FieldTable |
FieldManager.createFieldTableFromData(String fieldNamePrefix,
Unit ivarUnit,
Unit dvarUnit,
FieldVariable.ValueType dvarType,
double[] datapoints)
Creates a
FieldTable object with dependent and independent variables
FieldVariable . |
FieldTable |
Field.createTableInPart(BasePart targetPart)
Create a new table field from this field (regardless of type).
|
Modifier and Type | Method and Description |
---|---|
FieldLinksTable |
FieldManager.convertToLinksTable(FieldTable table)
Creates and returns a
FieldLinksTable representation of this table. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.