Package | Description |
---|---|
nxopen.fields |
Provides classes and interfaces for Fields.
|
Modifier and Type | Field and Description |
---|---|
static FieldEvaluator.LinearLogOptionEnum |
FieldEvaluator.LinearLogOptionEnum.LINEAR_LINEAR
Standard linear interpolation.
|
static FieldEvaluator.LinearLogOptionEnum |
FieldEvaluator.LinearLogOptionEnum.LINEAR_LOG
Independent variable scaling is linear, Dependent variable scaling is logarithmic (ln)
|
static FieldEvaluator.LinearLogOptionEnum |
FieldEvaluator.LinearLogOptionEnum.LOG_LINEAR
Independent variable scaling is logarithmic (ln), Dependent variable scaling is linear
|
static FieldEvaluator.LinearLogOptionEnum |
FieldEvaluator.LinearLogOptionEnum.LOG_LOG
Both Independent variable and Dependent variable scaling are logarithmic (ln)
|
Modifier and Type | Method and Description |
---|---|
FieldEvaluator.LinearLogOptionEnum |
FieldTable.linearLogOption()
Returns
the linear/log option used when this table data is evaluated using the linear 1d interpolator.
|
static FieldEvaluator.LinearLogOptionEnum |
FieldEvaluator.LinearLogOptionEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FieldEvaluator.LinearLogOptionEnum |
FieldEvaluator.LinearLogOptionEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FieldEvaluator.LinearLogOptionEnum[] |
FieldEvaluator.LinearLogOptionEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FieldTable.setLinearLogOption(FieldEvaluator.LinearLogOptionEnum linearOption)
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.