Package | Description |
---|---|
nxopen.fields |
Provides classes and interfaces for Fields.
|
Modifier and Type | Field and Description |
---|---|
static FieldEvaluator.InverseDistanceWeightingEnum |
FieldEvaluator.InverseDistanceWeightingEnum.ALL
Sum of the weighted value of all points, based on the inverse of the distance
|
static FieldEvaluator.InverseDistanceWeightingEnum |
FieldEvaluator.InverseDistanceWeightingEnum.NEAREST_POINTS
Sum of the weighted value of N nearest points (as a fraction of the total number of points), based on the inverse of the distance
|
FieldEvaluator.InverseDistanceWeightingEnum |
FieldTable.IdwOptionsData.nearestOption
nearest option
|
static FieldEvaluator.InverseDistanceWeightingEnum |
FieldEvaluator.InverseDistanceWeightingEnum.RADIUS
Sum of the weighted value of points within a radius (as a fraction of the bounding box diagonal), based on the inverse of the distance
|
Modifier and Type | Method and Description |
---|---|
static FieldEvaluator.InverseDistanceWeightingEnum |
FieldEvaluator.InverseDistanceWeightingEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FieldEvaluator.InverseDistanceWeightingEnum |
FieldEvaluator.InverseDistanceWeightingEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FieldEvaluator.InverseDistanceWeightingEnum[] |
FieldEvaluator.InverseDistanceWeightingEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
FieldTable.setIdwOptions(FieldEvaluator.InverseDistanceWeightingEnum nearestOption,
double nearestFraction)
Set the inverse distance weighting (IDW) interpolation options
License requirements: None. |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.