Package | Description |
---|---|
nxopen.fields |
Provides classes and interfaces for Fields.
|
Modifier and Type | Field and Description |
---|---|
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.ASTERISK |
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.CENTERLINE |
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.CIRCLE |
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.CROSS |
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.DIAMOND |
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.HIDE |
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.PLUS_SIGN |
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.POINT |
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.POUND_SIGN |
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.SQUARE |
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.TRIANGLE |
Modifier and Type | Method and Description |
---|---|
DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.showUndefinedValues()
Deprecated.
Deprecated in NX12.0.0. This method is deprecated. Use
DisplayPropertiesBuilder.showUndefValues() Undefined values are no longer displayed with various symbols, but are only on or off.
|
DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.tblIndepPtType()
Deprecated.
Deprecated in NX12.0.0. Table independent domain display no longer modifies the file and is included only to enable old journals to function without modification
DisplayPropertiesBuilder.showSrcTblVals() can be used to control source table values, but independent table values display is deprecated.
|
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DisplayPropertiesBuilder.ValuesEnum |
DisplayPropertiesBuilder.ValuesEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DisplayPropertiesBuilder.ValuesEnum[] |
DisplayPropertiesBuilder.ValuesEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DisplayPropertiesBuilder.setShowUndefinedValues(DisplayPropertiesBuilder.ValuesEnum showUndefinedValues)
Deprecated.
Deprecated in NX12.0.0. This method is deprecated. Use
DisplayPropertiesBuilder.showUndefValues() Undefined values are no longer displayed with various symbols, but are only on or off. For backward compatibility, calling this method with hide is the same as calling the new method with false; any other value is the same as calling the new method with true.
|
void |
DisplayPropertiesBuilder.setTblIndepPtType(DisplayPropertiesBuilder.ValuesEnum tblIndepPtType)
Deprecated.
Deprecated in NX12.0.0. Table Independent variable display no longer modifies the file and is included only to enable old journals to function without modification.
DisplayPropertiesBuilder.showSrcTblVals() can be used to show source table values, but independent table values display is deprecated.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.