Package | Description |
---|---|
nxopen.fields |
Provides classes and interfaces for Fields.
|
Modifier and Type | Field and Description |
---|---|
static DisplayPropertiesBuilder.TblPointTypeEnum |
DisplayPropertiesBuilder.TblPointTypeEnum.HIDE |
static DisplayPropertiesBuilder.TblPointTypeEnum |
DisplayPropertiesBuilder.TblPointTypeEnum.SHOW |
Modifier and Type | Method and Description |
---|---|
DisplayPropertiesBuilder.TblPointTypeEnum |
DisplayPropertiesBuilder.tblDepPtType()
Deprecated.
Deprecated in NX12.0.0. To show source table dependent values use
DisplayPropertiesBuilder.showSrcTblVals() to show source table values.
|
static DisplayPropertiesBuilder.TblPointTypeEnum |
DisplayPropertiesBuilder.TblPointTypeEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DisplayPropertiesBuilder.TblPointTypeEnum |
DisplayPropertiesBuilder.TblPointTypeEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DisplayPropertiesBuilder.TblPointTypeEnum[] |
DisplayPropertiesBuilder.TblPointTypeEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DisplayPropertiesBuilder.setTblDepPtType(DisplayPropertiesBuilder.TblPointTypeEnum tblDepPtType)
Deprecated.
Deprecated in NX12.0.0. Source table display no longer uses symbols, so this function has no meaning. Table values are only on or off; to show source table values use
DisplayPropertiesBuilder.showSrcTblVals() to show source table values.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.