Package | Description |
---|---|
nxopen.fields |
Provides classes and interfaces for Fields.
|
Modifier and Type | Field and Description |
---|---|
static DisplayPropertiesBuilder.DepDomColorEnum |
DisplayPropertiesBuilder.DepDomColorEnum.INHERIT |
static DisplayPropertiesBuilder.DepDomColorEnum |
DisplayPropertiesBuilder.DepDomColorEnum.SPECIFIED |
static DisplayPropertiesBuilder.DepDomColorEnum |
DisplayPropertiesBuilder.DepDomColorEnum.SPECTRUM |
Modifier and Type | Method and Description |
---|---|
DisplayPropertiesBuilder.DepDomColorEnum |
DisplayPropertiesBuilder.depDomColor()
Returns the dep dom color
License requirements: None. |
DisplayPropertiesBuilder.DepDomColorEnum |
DisplayPropertiesBuilder.tblDepDomColor()
Deprecated.
Deprecated in NX12.0.0. This function is deprecated, Tbl dependent Color can be chosen using
DisplayPropertiesBuilder.depDomColor() .
|
static DisplayPropertiesBuilder.DepDomColorEnum |
DisplayPropertiesBuilder.DepDomColorEnum.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static DisplayPropertiesBuilder.DepDomColorEnum |
DisplayPropertiesBuilder.DepDomColorEnum.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static DisplayPropertiesBuilder.DepDomColorEnum[] |
DisplayPropertiesBuilder.DepDomColorEnum.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
DisplayPropertiesBuilder.setDepDomColor(DisplayPropertiesBuilder.DepDomColorEnum depDomColor)
License requirements: None. |
void |
DisplayPropertiesBuilder.setTblDepDomColor(DisplayPropertiesBuilder.DepDomColorEnum depDomColor)
Deprecated.
Deprecated in NX12.0.0. This function is deprecated, Tbl dependent Color can be chosen using
DisplayPropertiesBuilder.depDomColor() .
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.