Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static WheelCoveringBuilder.SurfaceSectionType |
WheelCoveringBuilder.SurfaceSectionType.ADR42
The checking surface is created as ADR 42 type
|
static WheelCoveringBuilder.SurfaceSectionType |
WheelCoveringBuilder.SurfaceSectionType.CIRCLE_SECTION
The checking surface is created as circle section type
|
static WheelCoveringBuilder.SurfaceSectionType |
WheelCoveringBuilder.SurfaceSectionType.EXTRUDE_SECTION
The checking surface is created as extrude section type
|
Modifier and Type | Method and Description |
---|---|
WheelCoveringBuilder.SurfaceSectionType |
WheelCoveringBuilder.frontSurfaceSection()
Returns the surface section type of the front surface section.
|
WheelCoveringBuilder.SurfaceSectionType |
WheelCoveringBuilder.rearSurfaceSection()
Returns the surface section type of the rear surface section.
|
static WheelCoveringBuilder.SurfaceSectionType |
WheelCoveringBuilder.SurfaceSectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WheelCoveringBuilder.SurfaceSectionType |
WheelCoveringBuilder.SurfaceSectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WheelCoveringBuilder.SurfaceSectionType[] |
WheelCoveringBuilder.SurfaceSectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WheelCoveringBuilder.setFrontSurfaceSection(WheelCoveringBuilder.SurfaceSectionType frontSurfaceSection)
License requirements: nx_general_packaging ("NX General Packaging") . |
void |
WheelCoveringBuilder.setRearSurfaceSection(WheelCoveringBuilder.SurfaceSectionType rearSurfaceSection)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.