Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static WheelCoveringBuilder.SurfacePlaneType |
WheelCoveringBuilder.SurfacePlaneType.PERPENDICULARTO_LOADING
The checking surface is perpendicular to the active loading plane
|
static WheelCoveringBuilder.SurfacePlaneType |
WheelCoveringBuilder.SurfacePlaneType.WHEEL_PLANE
The checking surface is coplanar to the ourside of the wheels
|
Modifier and Type | Method and Description |
---|---|
WheelCoveringBuilder.SurfacePlaneType |
WheelCoveringBuilder.frontSurfacePlane()
Returns the surface plane type of the front surface section.
|
WheelCoveringBuilder.SurfacePlaneType |
WheelCoveringBuilder.rearSurfacePlane()
Returns the surface plane type of the rear surface section.
|
static WheelCoveringBuilder.SurfacePlaneType |
WheelCoveringBuilder.SurfacePlaneType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WheelCoveringBuilder.SurfacePlaneType |
WheelCoveringBuilder.SurfacePlaneType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WheelCoveringBuilder.SurfacePlaneType[] |
WheelCoveringBuilder.SurfacePlaneType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
WheelCoveringBuilder.setFrontSurfacePlane(WheelCoveringBuilder.SurfacePlaneType frontSurfacePlane)
License requirements: nx_general_packaging ("NX General Packaging") . |
void |
WheelCoveringBuilder.setRearSurfacePlane(WheelCoveringBuilder.SurfacePlaneType rearSurfacePlane)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.