Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static TireEnvelopeBuilder.SuspensionTemplateType |
TireEnvelopeBuilder.SuspensionTemplateType.FIVE_LINK_SOLID_AXLEWITHOUT_STEERING
Use the Five Link Solid Axle without steering suspension template.
|
static TireEnvelopeBuilder.SuspensionTemplateType |
TireEnvelopeBuilder.SuspensionTemplateType.MAC_PHERSON_STRUT
Use the MacPherson Strut suspension template.
|
static TireEnvelopeBuilder.SuspensionTemplateType |
TireEnvelopeBuilder.SuspensionTemplateType.SHORT_LONG_ARMWITH_STEERING
Use the Short-Long Arm with steering suspension template.
|
static TireEnvelopeBuilder.SuspensionTemplateType |
TireEnvelopeBuilder.SuspensionTemplateType.SHORT_LONG_ARMWITHOUT_STEERING
Use the Short-Long Arm without steering suspension template.
|
Modifier and Type | Method and Description |
---|---|
TireEnvelopeBuilder.SuspensionTemplateType |
TireEnvelopeBuilder.suspensionTemplate()
Returns the option to specify which suspension template will be used.
|
static TireEnvelopeBuilder.SuspensionTemplateType |
TireEnvelopeBuilder.SuspensionTemplateType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TireEnvelopeBuilder.SuspensionTemplateType |
TireEnvelopeBuilder.SuspensionTemplateType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TireEnvelopeBuilder.SuspensionTemplateType[] |
TireEnvelopeBuilder.SuspensionTemplateType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TireEnvelopeBuilder.setSuspensionTemplate(TireEnvelopeBuilder.SuspensionTemplateType suspensionTemplate)
License requirements: nx_general_packaging ("NX General Packaging") . |
void |
TireEnvelopeBuilder.setSuspentionTemplatePoint(TireEnvelopeBuilder.SuspensionTemplateType templateType,
int jointIndex,
Point3d pnt)
Change the location of a joint in the suspension template.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.