Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static TireEnvelopeBuilder.EnvelopeOffsetMethod |
TireEnvelopeBuilder.EnvelopeOffsetMethod.CUSTOMER_DEFINED_DATA
Use the data that the user defines.
|
static TireEnvelopeBuilder.EnvelopeOffsetMethod |
TireEnvelopeBuilder.EnvelopeOffsetMethod.FIXED_SECTIONS
Use the values in the fixed sections.
|
static TireEnvelopeBuilder.EnvelopeOffsetMethod |
TireEnvelopeBuilder.EnvelopeOffsetMethod.FROM_OFFSET_FILE
From the offset file.
|
Modifier and Type | Method and Description |
---|---|
TireEnvelopeBuilder.EnvelopeOffsetMethod |
TireEnvelopeBuilder.envelopeOffset()
Returns the option to specify which offset method is used in the envelope creation.
|
static TireEnvelopeBuilder.EnvelopeOffsetMethod |
TireEnvelopeBuilder.EnvelopeOffsetMethod.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TireEnvelopeBuilder.EnvelopeOffsetMethod |
TireEnvelopeBuilder.EnvelopeOffsetMethod.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TireEnvelopeBuilder.EnvelopeOffsetMethod[] |
TireEnvelopeBuilder.EnvelopeOffsetMethod.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TireEnvelopeBuilder.setEnvelopeOffset(TireEnvelopeBuilder.EnvelopeOffsetMethod offsetMethod)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.