Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static TireEnvelopeBuilder.DriverGraphOption |
TireEnvelopeBuilder.DriverGraphOption.BY_SKETCH
Use a sketch to define the driver.
|
static TireEnvelopeBuilder.DriverGraphOption |
TireEnvelopeBuilder.DriverGraphOption.RECTANGULAR_JOUNCE_REBOUND
Use the rectangular jounce rebound definition.
|
static TireEnvelopeBuilder.DriverGraphOption |
TireEnvelopeBuilder.DriverGraphOption.RECTANGULAR_TAPERED_X
Use the rectangular definition with taper in the X direction.
|
static TireEnvelopeBuilder.DriverGraphOption |
TireEnvelopeBuilder.DriverGraphOption.RECTANGULAR_TAPERED_Y
Use the rectangular definition with taper in the Y direction.
|
static TireEnvelopeBuilder.DriverGraphOption |
TireEnvelopeBuilder.DriverGraphOption.TAPERED_ONE_SIDE
Use the rectangular definition with taper on one side.
|
static TireEnvelopeBuilder.DriverGraphOption |
TireEnvelopeBuilder.DriverGraphOption.TWO_DRIVERS_ONE_FIXED
Use a fixed definition for two drivers.
|
Modifier and Type | Method and Description |
---|---|
TireEnvelopeBuilder.DriverGraphOption |
TireEnvelopeBuilder.driverGraph()
Returns the option to specify which driver definition is used in the suspension template.
|
static TireEnvelopeBuilder.DriverGraphOption |
TireEnvelopeBuilder.DriverGraphOption.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static TireEnvelopeBuilder.DriverGraphOption |
TireEnvelopeBuilder.DriverGraphOption.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static TireEnvelopeBuilder.DriverGraphOption[] |
TireEnvelopeBuilder.DriverGraphOption.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
TireEnvelopeBuilder.setDriverGraph(TireEnvelopeBuilder.DriverGraphOption driverGraphOption)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.