Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static SlopeBuilder.RequirementsControlType |
SlopeBuilder.RequirementsControlType.STANDARD_DRIVEN |
static SlopeBuilder.RequirementsControlType |
SlopeBuilder.RequirementsControlType.USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
SlopeBuilder.RequirementsControlType |
SlopeBuilder.requirementsControl()
Returns the requirements control for standard or user defined.
|
static SlopeBuilder.RequirementsControlType |
SlopeBuilder.RequirementsControlType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SlopeBuilder.RequirementsControlType |
SlopeBuilder.RequirementsControlType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SlopeBuilder.RequirementsControlType[] |
SlopeBuilder.RequirementsControlType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SlopeBuilder.setRequirementsControl(SlopeBuilder.RequirementsControlType requirement)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.