Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static SeatBeltAnchorageBuilder.LTwoLimitType |
SeatBeltAnchorageBuilder.LTwoLimitType.DEGREE45AND80
L2 limit angle area between 45 degree and 80 degree
|
static SeatBeltAnchorageBuilder.LTwoLimitType |
SeatBeltAnchorageBuilder.LTwoLimitType.DEGREE50AND70
L2 limit angle area between 50 degree and 70 degree
|
Modifier and Type | Method and Description |
---|---|
SeatBeltAnchorageBuilder.LTwoLimitType |
SeatBeltAnchorageBuilder.l2Limit()
Returns the l2 limit option
License requirements: None. |
static SeatBeltAnchorageBuilder.LTwoLimitType |
SeatBeltAnchorageBuilder.LTwoLimitType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeatBeltAnchorageBuilder.LTwoLimitType |
SeatBeltAnchorageBuilder.LTwoLimitType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeatBeltAnchorageBuilder.LTwoLimitType[] |
SeatBeltAnchorageBuilder.LTwoLimitType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SeatBeltAnchorageBuilder.setL2Limit(SeatBeltAnchorageBuilder.LTwoLimitType l2Limit)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.