Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static SeatBeltAnchorageBuilder.LOneLimitType |
SeatBeltAnchorageBuilder.LOneLimitType.DEGREE30AND80
L1 limit angle area between 30 degree and 80 degree
|
static SeatBeltAnchorageBuilder.LOneLimitType |
SeatBeltAnchorageBuilder.LOneLimitType.DEGREE50AND70
L1 limit angle area between 50 degree and 70 degree
|
Modifier and Type | Method and Description |
---|---|
SeatBeltAnchorageBuilder.LOneLimitType |
SeatBeltAnchorageBuilder.l1Limit()
Returns the l1 limit option
License requirements: None. |
static SeatBeltAnchorageBuilder.LOneLimitType |
SeatBeltAnchorageBuilder.LOneLimitType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeatBeltAnchorageBuilder.LOneLimitType |
SeatBeltAnchorageBuilder.LOneLimitType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeatBeltAnchorageBuilder.LOneLimitType[] |
SeatBeltAnchorageBuilder.LOneLimitType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SeatBeltAnchorageBuilder.setL1Limit(SeatBeltAnchorageBuilder.LOneLimitType l1Limit)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.