Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static SeatBeltAnchorageBuilder.ATLType |
SeatBeltAnchorageBuilder.ATLType.NO
hide ATL area
|
static SeatBeltAnchorageBuilder.ATLType |
SeatBeltAnchorageBuilder.ATLType.YES
show ATL area
|
Modifier and Type | Method and Description |
---|---|
SeatBeltAnchorageBuilder.ATLType |
SeatBeltAnchorageBuilder.atl()
Returns the atl option
License requirements: None. |
static SeatBeltAnchorageBuilder.ATLType |
SeatBeltAnchorageBuilder.ATLType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SeatBeltAnchorageBuilder.ATLType |
SeatBeltAnchorageBuilder.ATLType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SeatBeltAnchorageBuilder.ATLType[] |
SeatBeltAnchorageBuilder.ATLType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SeatBeltAnchorageBuilder.setAtl(SeatBeltAnchorageBuilder.ATLType atl)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.