Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static PedestrianProtectionBuilder.InternalBumperType |
PedestrianProtectionBuilder.InternalBumperType.BUMPER_BEAM_FACES
bumper beam faces method
|
static PedestrianProtectionBuilder.InternalBumperType |
PedestrianProtectionBuilder.InternalBumperType.BUMPER_TOP_PLANE
bumper top plane method
|
Modifier and Type | Method and Description |
---|---|
PedestrianProtectionBuilder.InternalBumperType |
PedestrianProtectionBuilder.internalBumperLineMethod()
Returns the method that should be used to create the internal bumper reference line
License requirements: None. |
static PedestrianProtectionBuilder.InternalBumperType |
PedestrianProtectionBuilder.InternalBumperType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static PedestrianProtectionBuilder.InternalBumperType |
PedestrianProtectionBuilder.InternalBumperType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static PedestrianProtectionBuilder.InternalBumperType[] |
PedestrianProtectionBuilder.InternalBumperType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
PedestrianProtectionBuilder.setInternalBumperLineMethod(PedestrianProtectionBuilder.InternalBumperType bumperMethod)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.