Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static ManikinBuilder.StandardType |
ManikinBuilder.StandardType.SAEJ826JUL1995
1995 SAE j826 Standard Type
|
static ManikinBuilder.StandardType |
ManikinBuilder.StandardType.SAEJ826NOV2008
2008 SAE j826 Standard Type
|
static ManikinBuilder.StandardType |
ManikinBuilder.StandardType.SAEJ833
SAE j833 Standard Type
|
static ManikinBuilder.StandardType |
ManikinBuilder.StandardType.USER_DEFINED
User Defined Manikin Size Type
|
Modifier and Type | Method and Description |
---|---|
ManikinBuilder.StandardType |
ManikinBuilder.standard()
Returns the standard used to define the manikin
License requirements: None. |
static ManikinBuilder.StandardType |
ManikinBuilder.StandardType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ManikinBuilder.StandardType |
ManikinBuilder.StandardType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ManikinBuilder.StandardType[] |
ManikinBuilder.StandardType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ManikinBuilder.setStandard(ManikinBuilder.StandardType standard)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.