Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static ManikinBuilder.PositionType |
ManikinBuilder.PositionType.DRIVER
Driver Type
|
static ManikinBuilder.PositionType |
ManikinBuilder.PositionType.PASSENGER
Passenger Type
|
Modifier and Type | Method and Description |
---|---|
ManikinBuilder.PositionType |
ManikinBuilder.position()
Returns the position of the manikin in the vehicle
License requirements: None. |
static ManikinBuilder.PositionType |
ManikinBuilder.PositionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ManikinBuilder.PositionType |
ManikinBuilder.PositionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ManikinBuilder.PositionType[] |
ManikinBuilder.PositionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
ManikinBuilder.setPosition(ManikinBuilder.PositionType position)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.