Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static HeadImpactAPillarDetailBuilder.MeasurementMethodType |
HeadImpactAPillarDetailBuilder.MeasurementMethodType.NOT_SPECIFIED |
static HeadImpactAPillarDetailBuilder.MeasurementMethodType |
HeadImpactAPillarDetailBuilder.MeasurementMethodType.ON_SURFACE |
static HeadImpactAPillarDetailBuilder.MeasurementMethodType |
HeadImpactAPillarDetailBuilder.MeasurementMethodType.WRAP_AROUND |
Modifier and Type | Method and Description |
---|---|
HeadImpactAPillarDetailBuilder.MeasurementMethodType |
HeadImpactAPillarDetailBuilder.measurementMethod()
Returns the measurement method used to position point 1.
|
static HeadImpactAPillarDetailBuilder.MeasurementMethodType |
HeadImpactAPillarDetailBuilder.MeasurementMethodType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static HeadImpactAPillarDetailBuilder.MeasurementMethodType |
HeadImpactAPillarDetailBuilder.MeasurementMethodType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static HeadImpactAPillarDetailBuilder.MeasurementMethodType[] |
HeadImpactAPillarDetailBuilder.MeasurementMethodType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
HeadImpactAPillarDetailBuilder.setMeasurementMethod(HeadImpactAPillarDetailBuilder.MeasurementMethodType measurementMethod)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.