Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static GroundClearanceBuilder.RequirementControls |
GroundClearanceBuilder.RequirementControls.STANDARD_DRIVEN |
static GroundClearanceBuilder.RequirementControls |
GroundClearanceBuilder.RequirementControls.USER_DEFINED |
Modifier and Type | Method and Description |
---|---|
GroundClearanceBuilder.RequirementControls |
GroundClearanceBuilder.requirementsControl()
Returns the value to determine what type of requirement is controlling the ground clearance values.
|
static GroundClearanceBuilder.RequirementControls |
GroundClearanceBuilder.RequirementControls.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static GroundClearanceBuilder.RequirementControls |
GroundClearanceBuilder.RequirementControls.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static GroundClearanceBuilder.RequirementControls[] |
GroundClearanceBuilder.RequirementControls.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
GroundClearanceBuilder.setRequirementsControl(GroundClearanceBuilder.RequirementControls requirementsControl)
License requirements: nx_general_packaging ("NX General Packaging") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.