Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Method and Description |
---|---|
CloseRangeDemoCylinderListItemBuilder |
CloseRangeVisibilityBuilder.createDemoCylinderListItemBuilder()
Creates a
CloseRangeDemoCylinderListItemBuilder
License requirements: nx_general_packaging ("NX General Packaging") Created in NX8.5.0 |
CloseRangeDemoCylinderListItemBuilder |
CloseRangeDemoCylinderListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
CloseRangeDemoCylinderListItemBuilder[] |
CloseRangeDemoCylinderListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
CloseRangeDemoCylinderListItemBuilderList.append(CloseRangeDemoCylinderListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
CloseRangeDemoCylinderListItemBuilderList.append(CloseRangeDemoCylinderListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
CloseRangeDemoCylinderListItemBuilderList.erase(CloseRangeDemoCylinderListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
CloseRangeDemoCylinderListItemBuilderList.erase(CloseRangeDemoCylinderListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
CloseRangeDemoCylinderListItemBuilderList.findIndex(CloseRangeDemoCylinderListItemBuilder obj)
Finds the index where the input object appears.
|
void |
CloseRangeDemoCylinderListItemBuilderList.insert(int location,
CloseRangeDemoCylinderListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
CloseRangeDemoCylinderListItemBuilderList.setContents(CloseRangeDemoCylinderListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
CloseRangeDemoCylinderListItemBuilderList.swap(CloseRangeDemoCylinderListItemBuilder object1,
CloseRangeDemoCylinderListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.