Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Method and Description |
---|---|
CloseRangeCameraListItemBuilder |
CloseRangeVisibilityBuilder.createCameraListItemBuilder()
Creates a
CloseRangeCameraListItemBuilder
License requirements: nx_general_packaging ("NX General Packaging") Created in NX8.5.0 |
CloseRangeCameraListItemBuilder |
CloseRangeCameraListItemBuilderList.findItem(int index)
Returns the object at the input index.
|
CloseRangeCameraListItemBuilder[] |
CloseRangeCameraListItemBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
Modifier and Type | Method and Description |
---|---|
void |
CloseRangeCameraListItemBuilderList.append(CloseRangeCameraListItemBuilder object)
Appends an object to the list
License requirements: None. |
void |
CloseRangeCameraListItemBuilderList.append(CloseRangeCameraListItemBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
CloseRangeCameraListItemBuilderList.erase(CloseRangeCameraListItemBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
CloseRangeCameraListItemBuilderList.erase(CloseRangeCameraListItemBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
CloseRangeCameraListItemBuilderList.findIndex(CloseRangeCameraListItemBuilder obj)
Finds the index where the input object appears.
|
void |
CloseRangeCameraListItemBuilderList.insert(int location,
CloseRangeCameraListItemBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
CloseRangeCameraListItemBuilderList.setContents(CloseRangeCameraListItemBuilder[] objects)
Sets the contents of the entire list.
|
void |
CloseRangeCameraListItemBuilderList.swap(CloseRangeCameraListItemBuilder object1,
CloseRangeCameraListItemBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.