Package | Description |
---|---|
nxopen.features.vehicledesign |
Provides classes and interfaces for Vehicle Design.
|
Modifier and Type | Field and Description |
---|---|
static BaseDataImportExportBuilder.OperateOptions |
BaseDataImportExportBuilder.OperateOptions.EXPORT |
static BaseDataImportExportBuilder.OperateOptions |
BaseDataImportExportBuilder.OperateOptions.IMPORT |
Modifier and Type | Method and Description |
---|---|
BaseDataImportExportBuilder.OperateOptions |
BaseDataImportExportBuilder.operateOption()
Returns the option which indicates if the spreadsheet is to be imported or exported.
|
static BaseDataImportExportBuilder.OperateOptions |
BaseDataImportExportBuilder.OperateOptions.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static BaseDataImportExportBuilder.OperateOptions |
BaseDataImportExportBuilder.OperateOptions.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static BaseDataImportExportBuilder.OperateOptions[] |
BaseDataImportExportBuilder.OperateOptions.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
BaseDataImportExportBuilder.setOperateOption(BaseDataImportExportBuilder.OperateOptions operateOptions)
License requirements: gateway ("UG GATEWAY") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.