public static class MirrorCertificationBuilder.ShowVisionConeType extends Enum
Modifier and Type | Field and Description |
---|---|
static int |
_ALL
Represents both of Eye-Mirror and Mirror Target vision cones are shown
|
static int |
_EYE_TO_MIRROR
Represents only Eye-Mirror vision cone is shown
|
static int |
_MIRROR_TO_TARGET
Represents only Mirror-Target vision cone is shown
|
static int |
_NONE
Represents the vision cones aren't shown
|
static MirrorCertificationBuilder.ShowVisionConeType |
ALL
Represents both of Eye-Mirror and Mirror Target vision cones are shown
|
static MirrorCertificationBuilder.ShowVisionConeType |
EYE_TO_MIRROR
Represents only Eye-Mirror vision cone is shown
|
static MirrorCertificationBuilder.ShowVisionConeType |
MIRROR_TO_TARGET
Represents only Mirror-Target vision cone is shown
|
static MirrorCertificationBuilder.ShowVisionConeType |
NONE
Represents the vision cones aren't shown
|
Modifier and Type | Method and Description |
---|---|
static MirrorCertificationBuilder.ShowVisionConeType |
valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static MirrorCertificationBuilder.ShowVisionConeType |
valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static MirrorCertificationBuilder.ShowVisionConeType[] |
values()
Returns an array that contains the values for this enum.
|
public static final MirrorCertificationBuilder.ShowVisionConeType NONE
public static final MirrorCertificationBuilder.ShowVisionConeType ALL
public static final MirrorCertificationBuilder.ShowVisionConeType EYE_TO_MIRROR
public static final MirrorCertificationBuilder.ShowVisionConeType MIRROR_TO_TARGET
public static final int _NONE
public static final int _ALL
public static final int _EYE_TO_MIRROR
public static final int _MIRROR_TO_TARGET
public static MirrorCertificationBuilder.ShowVisionConeType valueOf(int value)
public static MirrorCertificationBuilder.ShowVisionConeType valueOf(String name)
public static MirrorCertificationBuilder.ShowVisionConeType[] values()
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.