Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static SubdivisionSplitFaceBuilder.Types |
SubdivisionSplitFaceBuilder.Types.THROUGH_LINES
Through lines split type.
|
static SubdivisionSplitFaceBuilder.Types |
SubdivisionSplitFaceBuilder.Types.UNIFORM
Uniform split type.
|
Modifier and Type | Method and Description |
---|---|
SubdivisionSplitFaceBuilder.Types |
SubdivisionSplitFaceBuilder.type()
Returns the split type.
|
static SubdivisionSplitFaceBuilder.Types |
SubdivisionSplitFaceBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivisionSplitFaceBuilder.Types |
SubdivisionSplitFaceBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivisionSplitFaceBuilder.Types[] |
SubdivisionSplitFaceBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivisionSplitFaceBuilder.setType(SubdivisionSplitFaceBuilder.Types type)
License requirements: nx_subdivision (" NX SUBDIVISION") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.