Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static SubdivisionProjectCageBuilder.Types |
SubdivisionProjectCageBuilder.Types.ALIGN_NORMAL
Align edges normal to the specified plane
|
static SubdivisionProjectCageBuilder.Types |
SubdivisionProjectCageBuilder.Types.TO_AVERAGE
Project using best fit plane or axis
|
static SubdivisionProjectCageBuilder.Types |
SubdivisionProjectCageBuilder.Types.TO_TARGET
Project on target
|
Modifier and Type | Method and Description |
---|---|
SubdivisionProjectCageBuilder.Types |
SubdivisionProjectCageBuilder.type()
Returns the type
License requirements: None. |
static SubdivisionProjectCageBuilder.Types |
SubdivisionProjectCageBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivisionProjectCageBuilder.Types |
SubdivisionProjectCageBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivisionProjectCageBuilder.Types[] |
SubdivisionProjectCageBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivisionProjectCageBuilder.setType(SubdivisionProjectCageBuilder.Types type)
License requirements: nx_subdivision (" NX SUBDIVISION") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.