Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel |
SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel.BASE |
static SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel |
SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel.FIRST |
static SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel |
SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel.SECOND |
Modifier and Type | Method and Description |
---|---|
SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel |
SubdivisionPrimitiveShapeBuilderEx.sphereSubdivisionLevelOption()
Returns the subdivision level.
|
static SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel |
SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel |
SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel[] |
SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivisionPrimitiveShapeBuilderEx.setSphereSubdivisionLevelOption(SubdivisionPrimitiveShapeBuilderEx.SphereSubdivisionLevel level)
License requirements: nx_subdivision (" NX SUBDIVISION") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.