Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static SubdivisionPrimitiveShapeBuilder.Types |
SubdivisionPrimitiveShapeBuilder.Types.BLOCK |
static SubdivisionPrimitiveShapeBuilder.Types |
SubdivisionPrimitiveShapeBuilder.Types.CIRCLE |
static SubdivisionPrimitiveShapeBuilder.Types |
SubdivisionPrimitiveShapeBuilder.Types.CYLINDER |
static SubdivisionPrimitiveShapeBuilder.Types |
SubdivisionPrimitiveShapeBuilder.Types.RECTANGLE |
static SubdivisionPrimitiveShapeBuilder.Types |
SubdivisionPrimitiveShapeBuilder.Types.SPHERE |
static SubdivisionPrimitiveShapeBuilder.Types |
SubdivisionPrimitiveShapeBuilder.Types.TORUS |
Modifier and Type | Method and Description |
---|---|
SubdivisionPrimitiveShapeBuilder.Types |
SubdivisionPrimitiveShapeBuilder.type()
Deprecated.
Deprecated in NX11.0.0. Use
SubdivisionPrimitiveShapeBuilderEx instead.
|
static SubdivisionPrimitiveShapeBuilder.Types |
SubdivisionPrimitiveShapeBuilder.Types.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivisionPrimitiveShapeBuilder.Types |
SubdivisionPrimitiveShapeBuilder.Types.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivisionPrimitiveShapeBuilder.Types[] |
SubdivisionPrimitiveShapeBuilder.Types.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivisionPrimitiveShapeBuilder.setType(SubdivisionPrimitiveShapeBuilder.Types type)
Deprecated.
Deprecated in NX11.0.0. Use
SubdivisionPrimitiveShapeBuilderEx instead.
|
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.