Package | Description |
---|---|
nxopen.features.subdivision |
Provides classes and interfaces for Subdivision Body feature.
|
Modifier and Type | Field and Description |
---|---|
static SubdivisionExtrudeCageBuilder.DirectionType |
SubdivisionExtrudeCageBuilder.DirectionType.INFERRED |
static SubdivisionExtrudeCageBuilder.DirectionType |
SubdivisionExtrudeCageBuilder.DirectionType.PERPENDICULAR |
static SubdivisionExtrudeCageBuilder.DirectionType |
SubdivisionExtrudeCageBuilder.DirectionType.VECTOR |
Modifier and Type | Method and Description |
---|---|
SubdivisionExtrudeCageBuilder.DirectionType |
SubdivisionExtrudeCageBuilder.directionOption()
Returns the direction option
License requirements: None. |
static SubdivisionExtrudeCageBuilder.DirectionType |
SubdivisionExtrudeCageBuilder.DirectionType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SubdivisionExtrudeCageBuilder.DirectionType |
SubdivisionExtrudeCageBuilder.DirectionType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SubdivisionExtrudeCageBuilder.DirectionType[] |
SubdivisionExtrudeCageBuilder.DirectionType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SubdivisionExtrudeCageBuilder.setDirectionOption(SubdivisionExtrudeCageBuilder.DirectionType directionOption)
License requirements: nx_subdivision (" NX SUBDIVISION") . |
Copyright 2017 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.